This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: mmwave AllocationParam

Part Number: IWR6843ISK-ODS

Hi,

according to lab20 user guide, the AllocationParam has 4 parameters

the 1st is SNR threshold

the 2nd is velocity threshold

the 3rd is points threshold

the 4th is maxdistance

the 5th is maxvelocity

But according lab20 config file "mmw_pplcount_demo_default.cfg"

AllocationParam setting as below

AllocationParam 50 120 0.01 5 1 20

there are six parameters in this case

so what does the second parameter 120 mean?

Thansk

KuangMing Yin

 

  • Hi KuangMing,

    Old AllocationParams

    AllocationParam <SNR Threshold> <Min Velocity> <Points Threshold> <Max Distance> <Max Velocity>

    New:

    AllocationParam <SNR Threshold> <SNR Obscurd Threshold> <Min Velocity> <Points Threshold> <Max Distance> <Max Velocity>

    A track is considered obscured if an existing track is directly between it and the device. 

    Regards,

    Justin