This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA300: PGA300EVM-034

Part Number: PGA300
Other Parts Discussed in Thread: USB2ANY

Hello,

I'm measuring 0-10 Bar pressure with external piezoresistive sensor on PGA300EVM .

If pressure is 0 Bar DAC output 0.5 V

If pressure is 1 Bar DAC output 0.9 V

.............

If pressure is 10 Bar DAC output 4.5 V. This isn't a problem . Everything is OK. But;

For example;

I'm mesauring 10 Bar and Dac output is 4.5 V. I'm powers down of PGA300EVM-034. After I'm powers up the PGA300, DAC output is 0.5V . That's wrong because pressure is 10 Bar still. Dac output must be 4.5 V .

And I'm connected PGA300 via PC with USB2ANY. I'm switch Compensation mode after I'm activating OWI . And now DAC output is 4.5V, that's right. Do you understand me?

Briefly, can I use only pga300 without PGA300 GUI after programming with PGA300EVM GUI?