Other Parts Discussed in Thread: IWR6843
Hello,
My company is using the IWR6843 chip. We are working with CCS and mmwave_industrial_toolbox_3_6_0.
We are looking at lab0015_pplcount_68xx and lab0019_pplcount_long_range_68xx. We would like to understand these in detail. I understand that Lab 19 is intended to give approximately the same performance as Lab 15 BUT with longer range, (up to 50m). I have been studying the source code for these labs. I see that the source code is very similar but not identical for these 2 labs.
Could you give an overview of what is different in the source code between the 2 labs. Please explain what is changed in Lab 19 to give the longer range. It seems that more is changed than just configuration parameters. Can you reference specific files in each project and describe the main differences and how these differences give Lab 19 longer range?
Seeing the code differences which produce longer range will greatly help my understanding of how these labs function.
Thanks much,
Rob