Hello TI,
As per datasheet HDC2080 sensor is factory calibrated to rH accuracy of ±2% and temperature accuracy of ±0.2°C.
But we are not getting the accuracy as mention in datasheet. The results we are getting, are varying up to ±10% in rH and ±4°C in temperature.
I need to know :-
1. As per datasheet HDC2080 have the accuracy of ± 2% in rH and ±0.2°C in temperature then what is the significance of rH and temperature offset concept of up to ±25 % in rH and ±20.62 °C in temperature.
2. If the HDC2080 have the accuracy of ±2% in rH and ±0.2 °C in temperature then what is the need of offset.
3. The accuracy as you are mention in datasheet is with offset or without offset?