Am running expt with TDC7200EVM interfaced with Arduino UNO (SPI)
Ext clock : 64ns (in sync with source)
Ext Start: micro seconds (in sync with source)
Ext Stop: 32ns(in sync with source)
Am viewing the trigger out on an 20G sampling oscilloscope in persistence mode. The pulse width of the trigger out is varying in the range of 20ns to 10ms, as it can be seen from the below image.
my start signal has a constant pulse width of around 33ns. Then why is my trigger out pulse width varying?