Other Parts Discussed in Thread: TDC1000
Our interest is to find the differential time of fight (ToF) between two Ultrasonic Transducers placed apart at 10cm in Air/water medium. One of our clients gave two pair of sensors (Bina-1G2-1035 Ultrasonic transducer with Center frequency:975 ±30KHz & PSC1.0M02 2300 H2AD 4 B0 Ultrasonic flow sensor with nominal frequency 1.0±0.1MHz from ZHEJIANG JIAKANG ELECTRONICS CO., LTD.)for this ultrasonic application. We connected one of the wires of the Bina-1G2-1035 Ultrasonic transducer with the TDC1000-C2000 EVM at TX1 and another at GND in J5 connector. We didnt get corresponding changes in TDC avg window when the distance of the transducer is doubled. We are getting values around 37 micro second.
We need your support on the following: (i)Two Ultrasonic Transducers connection for Mode0, Mode1 and Mode 2 to find differential ToF and the corresponding settings required in the TDC1000 tab (ii)List of sensors that are compatible with this EVM and sensor specifications such as excitation frequency, excitation source voltage, Distance between the transducers, Resonance impedance and static capacitance.