Hello!
* There is an error in snoa963 [Inductive touch-ConfiguringLDC2114 Touch-Button sensitivity].
In the following text on page 8, is it correct to be 28 (DEC) instead of 0x28?
------------------------------------------------------------------------------------------------------------------
2. Let’s assume the I2C transaction in step 1 returned the value 0x28 (default) for the GAIN0 register. A
GAIN value of 0x28 corresponds to a gain factor of 11.5 according to Table 1 in the LDC2114 datasheet. This gain factor value (11.5) is the GAINnFACTOROLD term in Equation 1
--------------------------------------------------------------------------------------------------------------
Certainly 0x28 is the default value, but it should be 40 (DEC) in decimal. The above description needs to be modified. The example is not good.
Please let me know if the above is correct.
Best regards