This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Bhargav,
I would say that a 0.6A regulator is not sufficient for your 1.2A fan, but it's not really my place to speculate on these matters.The AMC6821 datasheet diagrams show that a discrete FET is needed to allow the AMC6821's PWM output to control the on/off state of the fan. This discrete FET would have some contribution to the voltage/current requirements of the fan circuit, but the AMC6821 itself would not contribute to this limit. If the source and FET are sufficient to switch the fan on/off, then the AMC6821 will be able to regulate fan speed.
thanks,
Ren
Thank you Ren for your quick reply!
We would like to elaborate more about our application. Fan start up current is attached below(this is captured without PWM control) and max current is 1.2A for 500ms duration and reaches 0.6A in normal spinning condition
Please refer to our application circuit diagram. Basically the Fan has 4 inputs pins for wiring. Two pins for power (12V ad GND) and two pins for PWM input and Tach output.
Our question is, Can we control the inrush current of 1.2A by programming the AMC6821SDBQR device?
12V Fan startup current without PWM control (12 V supply applied) :
Here is the proposed circuit :
No, you cannot use AMC6821 to stop the in-rush current. Toggling the fan's PWM input during start-up will only make the spin-up process take longer. If the fan needs 1.2A to start spinning, it won't prevent the peak current of 1.2A from occurring.
The spin-up feature of AMC6821 is intended to reduce fan noise.
Your schematic is missing the recommended FET between the PWM Out pin and the fan's PWM input.
thanks,
ren
Typically, the fan input is not a buffered, high impedance input and will take significant current to activate. AMC6821's open drain outputs are specified to sink up to 6mA (Vol spec in Electrical Characteristics table.) All of the functional diagrams in the datasheet depict this external, discrete FET for this reason. In the case of 2 and 3 wire fans, it is absolutely necessary to have the FET, because the only way to control speed is by controlling the fan's power supply directly.
As a digital pin, PWM out cannot exceed 6.5V per Absolute Maximum Ratings table on page 2 of the datasheet. This is further evidence that PWM out cannot be directly connected to a 12V pull-up resistor.
thanks,
ren