Other Parts Discussed in Thread: IWR1443, , IWR6843, TIDEP-0091,
Hi,
We are in process of selecting chipset for our application. Our application is quite power sensitive, We narrowed down on two chipset (IWR1443 and AWR1843).
I looked at the power consumption on their respective datasheets and power consumption estimate excel sheet for IWR1443, however I am looking at more detail information wrt power consumption and processing time (Something equivalent at the level of information provided in level sensing demo for IWR1443) to model battery life.
I am looking high accuracy demo and zone occupancy/area scanner demo to baseline power consumption comparison.
Please answer below question for AWR1843.
1) As AWR1843 has both HWA and DSP, application like High accuracy demo or Zone occupancy can be ported to either HWA or DSP. Can you provide details wrt power consumption(mA) estimates, processing time (in msec) estimates for the two applications(High accuracy demo and Zone occupancy demo) for case 1 : Running on HWA Case 2: Running on DSP. Which one is less power hungry and requires less time to process?
2) If the code is running on HWA, can DSP be powered down OR if code is running on DSP, Can HWA be powered down completely to save power. If so, Can you please provide instructions to power down HWA or DSP?
3) I noticed there is no high accuracy demo supported for AWR1843 or IWR6843, Can you provide instructions to port High accuracy demo for either AWR1843 or IWR6843 for power consumption measurements.
Thanks
Mahendra