Other Parts Discussed in Thread: PGA460
HI,
In a development project using PGA460, I chose a multiplexing scheme to mount multiple PGA460 onto the same serial port of the controller.However, this leads to a lot of extra overhead.So we want to be able to install PGA460 using a bus.
But I don't have a detailed description of this in the data book.After I successfully configured their UART_ADD and connected them to the UART, I found that I could not establish communication with them.However, if only one PGA460 is connected, the communication is normal.
The data from MCU to PGA460 goes through the following conversion process:
MCU <--MAX3232-->RS232<--MAX3232-->PGA460