Other Parts Discussed in Thread: AWR1443, AWR1642
HI:
I have two questions.
(1) We are using the AWR1243 for cascade design. We also looked at the published reference designs. The PDF file have two different parts, (i) AWR1243 and (ii) XWR1243.What is the difference in features between the two?
(2) The AWR 1243 Data sheet (SWRS188 –MAY 2017) shows that cascade is supported in AWR1243, when compared to AWR1443 and AWR1642. However, we are told now that ARW1243P variant of AWR1243 only supports cascading options. Is that true? We have already ordered the part AWR1243 (Part No: AWR1243FBIGABLRQ1). Is there anything that can be done? We can switch to AWR1243P parts in future. What can be done with the ordered parts? Besides incurring extra money for the new order, our design time is also extended. If there is any software fix, for using these parts, that would be greatful.
Regards
Ganesan