I am using LDC1101 with a custom made sensor and board.
I have attached inductor and capacitor(LC tank) as the same as LDC1101 EVM board.
My sensor has the size of 60mm*60mm, which is much larger than the sensor on LDC1101 EVM board.
However, the sensing distance is much shorter than the EVM board.
My goal is to achieve 20cm of sensing distance, but at the moment, I can only detect up to 5cm.
What could be the problem?