Can I have a clear explanation of Autozero. I am not sure exactly what is going on when this is set.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I have a clear explanation of Autozero. I am not sure exactly what is going on when this is set.
Fernando,
Please refer to the sections 8.3.6 Comparators for STOP Pulse Generation in the TDC1000 Datasheet.
The STOP pulse generation block of the TDC1000 contains two auto-zeroed comparators (a zero-cross detect and a threshold-detect comparator), a threshold setting DAC, and an event manager. Comparator auto-zero periods occur at the beginning of every TOF receive cycle. During these periods, the comparator’s input offset is stored in an internal 2.5-pF capacitor, and it is subtracted from the input signal during the echo processing phase. The duration of auto-zero period is configured with the AUTOZERO_PERIOD field located in the CLOCK_RATE register.
Fernando,
Please let me know which aspect of the auto-zero you need help with. Is it its implementation or usage ?
During these periods, the comparator’s input offset is stored in an internal 2.5-pF capacitor, and it is subtracted from the input signal during the echo processing phase.
What is the effect of the above? Reducing the signal? Making the signal zero for the period?
Fernando,
I will respond to your question by Friday this week. Sorry about this delay.
Thanks for the response. Also why is the THLD levels so far apart. If the echo and ringing is less than the steps then it will be challenging to discern the two.
Fernando,
Please let me know when are the THLD levels far apart? What is the steps that you point out here ?
Please provide me more about the setup that you have & try to measure the ToF, that can help me point you to the correct explanations for the same.
Level were a side note.. The main question was on autozero which up to now has not been properly explained.
Fernando,
Please refer to our FAQ on the Auto-Zero under the section "Auto Zero Period" https://e2e.ti.com/support/sensors/f/1023/t/724028. in detail.