Other Parts Discussed in Thread: AWR1642BOOST, UNIFLASH, AWR1642
Hi,
We are trying to capture data from AWR1642Boost using DCA1000 board. We have been able to set up mmwave studio and status of all the connections can be seen as Connected.
We are able to do all the steps starting from Set, Connect, Load BSS FW, Load MSS FW, SPI Connect, RF Powering successfully. When we hit run, a window pops up for downloading firmware to device. First time it shows that BSS FW is flashed successfully and the BSS firmware version is changed to 0.0.0.0(00/00/00) and MSS firmware doesn't flash at all. We are stuck at this point and unable to proceed. Attachment is the picture captured for the same scenario. Please help us.