Tool/software: Code Composer Studio
Hi,
For the real test,my configuration is shown belows:
The numbers of Tx and Rx Antenna are 3 and 4. The maximum range is configured as 130m.The CFAR threshold in the range and doppler direction are both 12 dB. In practical testing, the maximum detectble range is about 100m. Is there any configuration that is wrong?
I have another question, what are the differences between using 3tx antenna and 2tx antenna? Such as in performance, maximum detectable range etc.
Regards,
Rata