Other Parts Discussed in Thread: AWR1843, MMWAVE-DFP
How can I use the hardware frame trigger? does the trigger start a single frame or the multiple frames specified in the sensor config? do I need to ARM before i send each trigger or does it only need to be done once? do the data from multiple triggers get stored in separate bin files or in the same bin file? where is the pin to the trigger located? can I use a Raspberry Pi to trigger the frame?