Hi,
I am now trying to use IWR6843ISK-ODS radar device on Linux PC.
However, every time I connect it to the PC, Linux changes its device file names, for example, "/dev/ttyACM0", "/dev/ttyACM1", "/dev/ttyACM2" and so on, depending on the other usb devices connected.
I would like to distinguish its config and data ports among the other usb devices.
Is there any way to do that?
I expect that there must be some kind of HW specific number written in these two ports that Linux can read.
Best regards,
Fields