This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA305: PGA305

Part Number: PGA305

Work on this IC and with special code, the number basis is not defined, 24-bit coefficients are integer, with trying I think these are assumed to be fixed decimal point of 6, for example 1234567 can be calculated as 1.23456 is this correct? there is no description of the basis, for another example, without that assumption T^3 would overflow any 24-bits, can you provide the basis or the number range to allow us to continue and create a system around this IC. with thanks