Other Parts Discussed in Thread: AWR1642
Do you recommend that the CFAR Window and Guard length is fixed for all configurations of the AWR1642, or do you think that the window and guard length should increase if there are a higher number of samples in a configuration? For example, should the range CFAR window length of 8 and guard length of 4 for a test with 256 ADC samples per chirp be the same as in a test with 1024 ADC samples per chirp?