Hi expert.
My name is Jeong.
I want to detect (tx1-tx2) 60m and (tx3) 200m using the advanced frame.
The following configuration has led to a strange phenomenon.
sensorStop
flushCfg
dfeDataOutputMode 3
channelCfg 15 7 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 61 3 1 41 0 0 4 1 256 6500 0 0 48
profileCfg 1 61 3 1 100 0 0 6 1 256 2689 0 0 48
chirpCfg 0 0 0 0 0 0 0 4
chirpCfg 1 1 0 0 0 0 0 0
chirpCfg 2 2 1 0 0 0 0 1
chirpCfg 3 3 1 0 0 0 0 2
advFrameCfg 2 0 0 1 0
subFrameCfg 0 0 0 2 128 100 0 1 1 100
subFrameCfg 1 0 2 2 64 100 0 1 1 100
1) ProfileCfg 0 is 200m, but all subframes( 0 and 1) are detected 60m (profilecfg 1).
2) If profileCfg 1 is changed to 100m, all subframes detect 100m.
3)If the chirpCfg is changed as follows, the radar does not operate.
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
chirpCfg 2 2 1 0 0 0 0 4
chirpCfg 3 3 1 0 0 0 0 0
Please tell me the advanced frame configuration used by dividing tx1-tx2, tx3.