This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AWR1843BOOST: Extending the unambiguous velocity measurement range using the function disambiguateVel

Part Number: AWR1843BOOST

Tool/software: Code Composer Studio

Hi,

   In the MRRdemo,there is a function called disambiguateVel which extends the unambiguous velocity measurement range  by 3x. There are two type chirps,fast chirp period is 65us, and slow chirp period is 78us.Why is disambiguation of up to 3x of the naive max-velocity obtained by the above configuration according to chinese remainder theorem?

Thanks,

Regards,

Rata