This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Ethernet communication to/from the IWR6843

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843, MMWAVEICBOOST, MSP432E401Y

Hi,

We are interested in using IWR6843 with an external device which supports communication using Ethernet or WiFi. Is it possible to use the MSS on IWR6843 to send Ethernet packets? If yes can you please provide some more information on that. If not do you have any recommendations of processors to be used with IWR6843 which can take the data over UART and transmit over Ethernet as well as do some additional processing also.

Regards,

Attiya