This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/IWR1642BOOST: How to run demo of xwr16xx of SDK 3.2 on CCS?

Part Number: IWR1642BOOST


Tool/software: TI C/C++ Compiler

Hi guys,

I just downloaded the new version of SDK 3.2 and I want to implement the demo for xwr16xx into CCS, however, when I "import the existing project" on CCS there are no files to be selected. I was able to do it with the demo for driver vital sign I can see there are 2 files dss and mss to be selected. These 2 files have the type of PROJECTSPEC so I guess CCS can detect them but not the same case for the demo of xwr16xx with different types. I want to ask for your help on this problem to run the demo of xwr16xx.

Thanks for your help!