Hi. I have been using the DCA-1000EVM board for a week or so now.
Everything has been working perfectly fine, but I needed to change the test environment, so I moved the board to a new computer and tried setting up the board again.
I did everything same as I did before, but this time the board started to malfunction, with the message, a problem was encountered while attempting to add the driver.
After a few trials, I connected the board back to the original setup computer, but it seems like the board is not working on the original computer as well (with the same message, and FTDI not being recognized.)
Is there a possibility that the FTDI chip was damaged by some reason? (There was no physical damage to it.)
Or, maybe if it is the problem with the board, is there a way for me to perhaps reset the DCA1000EVM board completely?
Thank you.