This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Can I use multi frequency for MIMO?

Part Number: IWR6843
Other Parts Discussed in Thread: MMWAVE-SDK

Hi

I notice that from the IWR6843 tech book, there is a saying "While the IWR6843 has three transmitters, only two of them are utilized in a TDM (time-division multiplexing)-MIMO(Multiple-Input-Multiple-Output) fashion during a frame."

This is great! But I STILL wonder how the IWR 6843 MIMO work. Can it work in different frequencies? For example, with MIMO, I suppose that there are two channels, but can those two channels work in different frequency at the same time? One in 60 GHz and the other one work in 64 GHz? 

Looking forward to your reply.

Jingxiao