Other Parts Discussed in Thread: OPT9221
Hello,
we are currently working on a new prototype using the OPT8241-CDK-EVM. After we tried to transfer a camera profile including Pixel-Wise calibration Data to the EVM, no connection can be established between the device and the Voxel Viewer (0.9.10) anymore.
* If the EVM module is connected to the host before starting the Voxel Viewer, the Voxel-Viewer software crashes at startup.
* If the Voxel-Viewer software is started first, then the EVM is connected, the module appears in the device selection list. If this module is selected and confirmed by a click on "Ok", the Voxel-Viewer crashes.
* There are no entries in the Voxel-Viewers log file
The OPT9221 firmware has been already flashed to 0.31 (the "Voxel-programmer" is still working). We suspect that the CDK-FX2 firmware has to be renewed/updated. Where can we get it? Are there any other measures we can take?
Best regards,
Patrick