This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Vital Signs example not working with IWR6843-AOP standalone configuration

Part Number: IWR6843AOPEVM
Other Parts Discussed in Thread: MMWAVEICBOOST

Hi,

When configure IWR6843-AOP EVM in standalone mode and try to run Vital Sign lab, after launch VitalSignsRadar_Demo GUI application, the UART/data COM port can't be detected correctly nor can be COM port changed under setting dialog. But, when IWR6843-AOP mount with MMWAVEICBOOST EVM and configure in BOOST mode, the VitalSignsRadar_Demo application can be launched and running correctly. So, is there a fix to make Vital Sign demo working in AOP standalone mode? Thanks!

Regards,

Ken Hsieh