In the PKG drawing on page 58 of data sheet. Lead thickness is showen as (A) TYP, and Table of DIM A shows two opt 1 which is 0.1 and 0.2.
I would like to know default of lead thickness. Is this 0.1 or 0.2 ? Pls refer to below.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In the PKG drawing on page 58 of data sheet. Lead thickness is showen as (A) TYP, and Table of DIM A shows two opt 1 which is 0.1 and 0.2.
I would like to know default of lead thickness. Is this 0.1 or 0.2 ? Pls refer to below.
Hello,
Unfortunately your image didn't come through. Could you reattach?
Best Regards,
Hello,
I've reached out to our packaging department, and the QFN packages can be constructed with leads of either thickness (neither is default). You should account for both possible lead thicknesses.
Best Regards,
Dear Kristin Jones
Thank you very much for answering to my question. I unerstand no deafault.
By the way, Will you let me know the reason RGH provide 2 option for leadframe thickness ? while leaddframe thickness of other PKG like RTE16 is 0.2 only.
Best regards,
M. Suzuki
Hello,
Unfortunately I do not know why there are two options. I only know that there are two leadframe thickness options.
Best Regards,
Dear Kristin Jones
Thank you for reply.
Lastly I want confirm how does customer specify lead thciness.
Does customer have to specify lead thickness when order LDC1614-Q1 ?
Best regards,
M. Suzuki
Hello Suzuki-san,
My apologies for the delayed reply. I was on vacation all of last week.
No, your customer does not have to specify lead thickness when ordering the LDC1614-Q1.
Best Regards,