hi,
In LMP91000 datasheet is not very clear to us how VOS_RW is measured.
Our believe is that:
- VOS_RW = -550uV;
- Bias = 0V;
- Internal Zero=50% VCC (3.3V/2 = 1.65V);
- RL = 10 Ohm;
- TIA_GAIN = 35k;
- 3-electrode sensor is connected with zero output current;
- LMP91000 in 3-electrode Amperometric mode;
Offset voltage between RE and WE causes current to flow into TIA through 10 Ohm resistor (-550uV/10 Ohm = -55uA), then TIA gain current for 35k (55uA*35k = 1.925V), Vout achieves GND rail and cutted-off, cause we use Vcc=+3.3V.
Currently with our samples of LMP91000, VOS_RW is very small, but during manufacturing, is probability that we have samples with -550uV offset, which is a no-go for our apps.
Any advice is more than welcome
KR
Vincenzo