Hi
I am working on IWR1443 custom board,I successfully bring up the board and its running demo code. (Tested via UART)
We have an RS485 interface for both config port and Data port. For this, I added below code in cli.c, after added I compiled cli library too.
"ti/mmwave_sdk_02_01_00_04/packages/ti/utils/cli/cli.c"
After these changes, the board is not booting up, kindly help us to resolve this issue.
SDK Version: mmwave_sdk_02_01_00_04
And One more question: can I use XDS100v2 debugger for IWR1443
Regards,
Ravi