This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: LDC1612

Part Number: LDC1612

Hi,

Can I have more than one LDC1612 on a I2C bus.  I'm new to the I2C bus and don't see a way to address individual devices.

Thanks

  • Hello,

    You can have up to two LDC1612 devices on the same I2C bus. There are two possible I2C addresses, which you can select by tying the ADDR pin high or low. If you need to have more than two LDC1612s on the same bus, you would need to use an I2C expander. 

    Best Regards,