Other Parts Discussed in Thread: IWR6843, IWR1843, , TMP112, IWR1642
Hi mmwave champs,
When powering up the IWR6843 board directly (without using the boost kit) the consumption is already 330mA (3.3v) without starting to initiate the radio.
Q1 : Is such power consumption expected ?
Q2 : What does it correspond to in term of power consumption (CortexR4F only)?
Q3 : More generally, even if it is not specified in the datasheet yet, what are the expected power consumptions on IWR6843 (no radio, 1 Tx/4 Rx, …)?
Q3bis : Should we expect similar consumptions shown on the IWR1843 datasheet?
Thank you!
Best regards,
Guillaume