Hi Technical Support
C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0013_traffic_monitoring_16xx\gui\tm_demo.m
Is there a process that is not detected near the radar?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Technical Support
C:\ti\mmwave_industrial_toolbox_3_6_2\labs\lab0013_traffic_monitoring_16xx\gui\tm_demo.m
Is there a process that is not detected near the radar?
Dear Amanda
Thank you for reply.
And, thank you for telling me about related threads.
> 1. The range resolution of the MIMO configuration is only 0.25m. In the processing chain, the first few range bins are discarded from detection due to FFT leakage.
Best Regards
Hello,
The DC calibration function is detailed in the doxygen of the mmWave SDK documentation. The first few range bins are affected by FFT leakage. I would recommend to evaluate close distances by using the Out of Box demo instead of the traffic monitoring demo. In addition, the latest TM demo using 6843 or 1843 are recommended for compatibility with the latest SDK. Please consider using this demo instead if you need more customization for short ranges.
Amanda