This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Jim,
Although your images didn't come through, I received an email from Noah with the images attached and was able to view them. I think it's unlikely that slight differences in the trace lengths would affect this. The excitation signal is very low frequency (typically 25kHz), so length matching is not necessary.
Can you share your measurement configuration? I'd like to verify that SHLD1 is the correct shield for both electrodes. If you are only using single-ended measurements, SHLD1 and SHLD2 are shorted internally, but they are 180 degrees out of phase for differential measurements. If you are using differential measurements you might see some error due to additional capacitance on one electrode.
Also please note that I'll be on vacation tomorrow through the end of next week, so my responses will be delayed until I return.
Best Regards,
Hi Kristin,
Thanks for your quick response. It's good to confirm my suspicions that the length difference shouldn't be a big issue.
Did you see any other issues with our layout technique of interleaving shield traces between the sense channels?
As for our configuration, we are only using channels one and two, and we are configured for single ended measurements and assume shield 1 and 2 are internally shorted as you note.
Hi Kristin Jones93 do you have any other feedback on our layout above?
Hi Jim,
My apologies for the delayed reply. I was on vacation all last week.
I don't remember seeing any layout problems when I last looked at it, but I will double check and get back to you this week.
Best Regards,
Hi Jim,
I've double checked your layout, and I don't see any problems with it. You may see some improvement by eliminating the header, which can't be effectively shielded. Otherwise I don't see any potential sources of error in the layout.
Best Regards,