This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2214: Is FDC 2214 a sensor itself that can be attached to the cooling body?

Part Number: FDC2214

Dear Sir/Madam,

Is FDC2214  is a capacitive sensor itself that can be attached to the cooling body? Do I need to purchase an FDC2214EVM  to connect to FDC2214 for sensing the capacitive change? 

I have no knowledge of designing the board or customise the sensor myself, I wish to buy in a set that can is ready to use.

Best Regards,

QiuPing