This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: ERRB Pin going low after power up without a new measurement starting.

Part Number: TDC1000

Are there any suggestions as to why the ERRB pin would go low after initialization? Reading the  ERROR_FLAGS register shows  the result of 0x00 (no errors) which makes sense since I am testing the device with no TRIGGER signal and in the default setup. During startup I have probed this pin and it starts off with 3.3V volts then immediately goes to 0V after being enabled, the appropriated pull up resistor circuit for topen drain operation is also being used.