Hi E2E,
Good day.
According to the HDC2080 datasheet, the temperature accuracy is typically +/-0.2 °C to +/-0.4°C, however, the test condition is at 5°C < TA < 60°C. The temperature sensor has an operating range from -40°C to 125°C, I would like to confirm if the temperature accuracy is true from -40°C to 5°C? and for the entire operating temperature range?
Regards,
Carlo