Hi All,
I need to implement a contactless position sensor, to measure absolute linear position over a 45cm stroke, accuracy of ~1mm.
At first glance, an Inductive to Digital Converter (like the LDC1612) coupled with a rectangular streched coil looks a good candidate, however, looking at the "Inductive sensing FAQ" section in the E2E support forum this solution is not recommended for distances greather than 10cm.
I was wondering if the 10cm limitation can somehow be overcomed.
what's the rationale behind that maximum value and can it be overcomed, playing with the coil geometry?
is there any other technique more suitable for contactless linear position measurements over a such long distance (45-50cm) ?
Thanks in advance