This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA305: Beginner question with PGA305

Part Number: PGA305
Other Parts Discussed in Thread: ADS122C04

Hello,

I believe the PGA305 is the correct choice to integrate into our product.  Forgive me as a beginner but there are some basics that I am having trouble to understand.  I just want to read the resistance of a sensor.  The resistance ranges from 1Kohm to 100Kohm.  In the bridge design then I was planning to use 3 of the resistors at a fixed value, say 50Kohm and the 4th would be my sensor that has an unknown resistance.  I want to read the PGA305 with I2C, which register do I read to get the information necessary to calculate the unknown resistance of my sensor?

Thanks,

Steve