Hi again,
Provided the config register is set to positive edge trigger for the start/stop signals, is it then required to provide these signals as pulses as for example shown in figure 16 of the datasheet? Or can the been held high after the transition? Of course signals have to return to low before a new measurement can be started - but this is not the issue here. I just want to know whether there is a requirement for the start signal to be low before a low to high transition on the stop signal can be detected.
Assuming start/stop signals are truly edge triggered the signal state after the transition should not matter at all, but the datasheet always shows the start/stop signal return to low within a clock cycle - hence my doubt.
Best regards
Klaus