Dear all ,
I'm testing the AWR1642BOOST Eval Kit, I would like to connect it to the CAN BUS. It's obviously that the AWR1642BOOST uses CAN-FD connector.
Does AWR1642BOOST support CAN-HS ?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all ,
I'm testing the AWR1642BOOST Eval Kit, I would like to connect it to the CAN BUS. It's obviously that the AWR1642BOOST uses CAN-FD connector.
Does AWR1642BOOST support CAN-HS ?
Thank you
Hello,
The device supports it but the pins are not brought out to a connector or CAN PHY. The pins for DCAN (same as CAN HS) are brought to the 60 pin connector, which has series resistors on each signal. You could connect a wire to the pad for the series resistor and connect to an external CAN Phy if you want.
Regards,
adrian