Other Parts Discussed in Thread: IWR1642BOOST, , IWR1642
Hi,
I bought the IWR1642BOOST first and tested for people counting. The accuracy of the IWR1642BOOST was excellent for my application. In the next step I bought the AoP module from Mistralsolution. This module use IWR6843AoP . I have tested it, but accuracy AoP module was low for my application. I think the low accuracy of AoP module due to the angular resolution and signal strength.
Now I want to buy 60GHz AoPCB from Mistralsolution. It use IWR6843 IC and Antenna on pcb similar to IWR1642BOOST.
- Can it be said that the accuracy of AoPCB from Mistralsolution is in all respects similar to IWR6842BOOST?
- Can I use AoPCB instead of IWR6842BOOST ?
Thanks