Hello. I’m trying to estimate the 3D location of the object using IWR6843ODS + DCA1000 data, but my results seem upside down.
There is no problem with Azimuth-angle FFT.
When an object is located on the left side (location with positive azimuth angle) of the sensor ( the position is specified in the above figure), the peak appears at (+vres), after 4-point FFT.
However, the result of elevation-angle fft is upside down.
When an object is located on the top (location with a positive elevation angle), the peak appears at (-vres).
Also, when it is located on the bottom (location with a negative elevation angle) the peak appears at (+vres).
Do you know what caused this error?
I don’t think it is code error, because the result is accurate for azimuth angle direction.
Is the TX/RX number above incorrect?