Other Parts Discussed in Thread: LDC2114
I am working on a flow meter that has a dial with a rotating needle calibrated to measure the water flow. I wanted to use LDC0851 to generate an interrupt to count the rotations of the needle. The flow meter is battery operated which requires the sensor to be in Low power mode. But the challenge i am facing is that the water flow through the meter is varying and to work in Low power mode EN pin of the sensor need to be duty cycled with a constant time interval between the on and off time of the sensor (as i have inferred from the datasheet) which is not possible in our case since the dial rotation is varying with varying water flow.
Please help me to find a solution.