This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: Radome boost signal

Part Number: IWR6843ISK

Hi Ti,

In our lab, I have IWR6843ISK aiming towards big metal corner reflector (e.g 5m apart). There are no other object at 5m distance. I use mmWaveDemoVisualizer to visualize Relative Power (dB) of the reflector. I would like to use this graph to estimate correct thickness of the radome wall. Unfortunately it seems that the graph is adjusting in some way - when I place radome in front of the radar, the energy from corner reflector always rises (which is I guess not possible).

Is there any way I can display true value of the peaks?

Thank you, Lukas