{
/* Master */
{ /* TX1, TX2, TX3 - {Azimuth offset, Elevation offset (in lambda/2)} */
{11U, 6U}, {10U, 4U}, {9U, 1U}
},
/* Slave 1 */
{ /* TX1, TX2, TX3 */
{32U, 0U}, {28U, 0U}, {24U, 0U}
},
/* Slave 2 */
{ /* TX1, TX2, TX3 */
{20U, 0U}, {16U, 0U}, {12U, 0U}
},
/* Slave 1 */ // I think there is a typo here in the SDK. It should be Slave 3
{ /* TX1, TX2, TX3 */
{8U, 0U}, {4U, 0U}, {0U, 0U}
}
};
{
aoa_sensorRxOffset[1].sensorAzimOffs = 11;
aoa_sensorRxOffset[2].sensorAzimOffs = 50;
aoa_sensorRxOffset[3].sensorAzimOffs = 46;
aoa_sensorRxOffset[1].sensorAzimOffs = 50;
aoa_sensorRxOffset[2].sensorAzimOffs = 46;
aoa_sensorRxOffset[3].sensorAzimOffs = 0;