Other Parts Discussed in Thread: , , MMWAVE-SDK,
Hi, The mmwave SDK out of box demo for the IWR6843 EVM consists of two versions that is one is by using the on chip DSP and HWA (on-chip Hardware Accelerator) which is supported by IWR6843ISK. The other one is just by using the HWA(on-chip Hardware Accelerator) supported by IWR6843ISK and IWR6843AOPEVM. May i know how these two different software versions of the out of box SDK influence the output of the sensor.
The out of box demo for the IWR6843ISKODS is a point cloud visualizer through which the output of the sensor can be visualized in the zone occupancy visualizer lab GUI. May I know why isn't their a SDK for the IWR6843ISKODS which enables visualization of the output in the web-based mmWave Demo Visualizer.