This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: What is the Minimum Range we can measure with High Accuracy Example?

Part Number: IWR1443
What is the minimum range we can measure with High Accuracy Lab example?
As per the documentation
RangeLimitCfg 1 x  y  (With This configuration iwr1443 finds the object and measures the range in between x meters and  y meters)
In High Accuracy config fileRangeLimitCfg 1 0.5  3.0 (Means IWR1443 can find the object in between 0.5m(50cm) and 3.0(300cm)). 
With the above we are able to get the object range correctly in between 50cm and 300cm .
 
Now we want measure the range of objects from 5cm  to 500cm. We tried with RangeLimitCfg 1 0.01  5.0 ( Here Min is 0.01m= 1cm, Max is 5.0m=500cm).we are getting 1cm every time.
With same configuration we changed the object range upto 50 cm -200cm, this time also it's giving 1cm most of the time.
If we change Min as 0.2 (20cm) - RangeLimitCfg 1 0.2  5.0 , getting correct results in between 20cm to 500cm.
So, can't we measure the  2-5 cm range objects with IWR1443?
What is the minimum range we can measure with High Accuracy Lab example?
What are the changes we need to make to measure the 2-5cm range objects?
Regards,
Harish.