This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243: external clock

Part Number: AWR1243

Hello team,

I have the following questions:

1. Can external PLL/VCO be used instead embedded 20 GHz PLL synthesizer? The AWR1243 on-chip synth. has very poor phase noise performance. Anyway, in cascaded application only one PLL synth work, while other just sleep. So, why not to use external high-quality chirp modulated PLL source with sync signal for all chips? If necessary, the same 40 MHz clock may be used as clock for the external PLL and AWR1243.

2. Can we recommend a high quality GaAs mmW LNAs between receive antennas and receiver inputs of the AWR1243? The 15dB noise figure for AWR1243 is high compared to some external devices with 3.6 dB. What max RF input level to avoid the AWR1243’s LNA being broken?

3. For multichip mmW cascading much easy to use separate chips on transmit and receive. It allows flexible separation and better isolation of the transmit and receive antennas arrays. Can we use the AWR1243 in receive or transmit mode only, by disabling excessive function to save the power?  

4. For MMWAVCAS-RF-EVM eval. board with four AWR1243P. How much the RF feed losses are? 

Thanks!

Errol

  • Hello Errol,

    1.) You cannot use an external VCO  because you need to synchronize the FMCW ramp to the AWR devices framing engine. How will you determine the start of the ramp , end of the ramp etc. in the external VCO? The phase noise performance of the AWr1243 is best in class among the integrated CMOS FMCW radar solutions available today.

    2) You could use external LNA. You will need to make sure the internal Rx chain does not go into saturation (ADC data does not saturate). This amplitude will depend on the Rx gain you have configured in the AWR device. Its recommended to be atleast 6dB below ADC full scale (ADC full scale is 1Vpk at the ADC input).

    3) You can completely control the Tx and Rx you want to operate in the chip. The static config API allows you to set that.

    4) Do you mean the trace losses from antenna to device ball ? On the Rx paths the trace loss is ~ 2.1 dB and Tx paths is ~1.6 dB.

    regards,

    Vivek