This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: IWR6843

Part Number: IWR6843
Other Parts Discussed in Thread: , MMWAVEICBOOST

I  want to make Radar using IWR6843. It should detects obstacle in its range and also calculate the distance from the object. Can it be done?

Also is this a pulse radar and what is the max-distance this radar can measure? If this radar is not good for this project, what radar do you suggest?

  • Hi Nasir,

    IWR6843 is going to be a great fit for your application, I would recommend ordering an IWR6843ISK and MMWAVEICBOOST in order to begin evaluation.

    This is not pulse radar, but rather Frequency Modulated Continuous Wave Radar. You can read more about the technology here.

    Let me know if you have more questions.

    Cheers,

    Akash